cancel
Showing results for 
Search instead for 
Did you mean: 

Motor profiler does not work in 6.3.2 while it is in 5.4.8

JulienD
Senior

Hello

 

I'm evaluating B-G431B-ES1 design.

As I don't have accurate specifications for the motor, I'm going through motor profiler.

 

If I use SDK 5.4.8, profiling seems to work. At least, the motor turns.

If I use SDK 6.3.2, profiling whistles while keeping the "startup beep-beep" but the motor never starts. Before that, I built a firmware with the motor profile option activated.

 

What did I miss?

Thanks

Julien

10 REPLIES 10
JulienD
Senior

Test 1:

- I removed esc feature.

- opened motorpilot

- loaded gui SimpleAppMCPV2.qml

- error -> this gui does not support motor profiling app (something like this).

- removed motor profiler from "application configuration" tab 

- restart gui.

- motor runs smoothly.

Is it what you requested?

 

Test 2:

- no motor profiler in app configuration

- esc enabled

-  potentiometer enabled

-> with this configuration, the motor does not start with the button, whatever the position on the potentiometer.