2024-11-25 06:17 AM
Hello
I'm evaluating B-G431B-ES1 design.
As I don't have accurate specifications for the motor, I'm going through motor profiler.
If I use SDK 5.4.8, profiling seems to work. At least, the motor turns.
If I use SDK 6.3.2, profiling whistles while keeping the "startup beep-beep" but the motor never starts. Before that, I built a firmware with the motor profile option activated.
What did I miss?
Thanks
Julien
2024-11-28 10:05 AM
Test 1:
- I removed esc feature.
- opened motorpilot
- loaded gui SimpleAppMCPV2.qml
- error -> this gui does not support motor profiling app (something like this).
- removed motor profiler from "application configuration" tab
- restart gui.
- motor runs smoothly.
Is it what you requested?
Test 2:
- no motor profiler in app configuration
- esc enabled
- potentiometer enabled
-> with this configuration, the motor does not start with the button, whatever the position on the potentiometer.