2014-01-23 7:00 AM
ST�s motor control software development kit provides all you need for the development of your motor control application based on the STM32 F0, F1, F2, F4 and now F3 (release v3.4) MCUs. It supports up to two PMSMs using any combination of current reading topologies and speed/position sensors, including sensorless operation. Application development and optimization is facilitated by the PC based MC Workbench software. This GUI sets SDK parameters, real-time access to control variables including their display on a virtual oscilloscope. Gigi #stsw-stm32100-pmsm-foc-sdk
2014-12-12 4:59 AM
Ciao
We are trying to simplify the download of the web distribution avoiding registration. Anyhow you can get only the last version and so the v4.0 (up to now). Download the older version like v3.3 is non possible. Ciao Gigi2014-12-12 8:11 AM
2021-06-21 9:25 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards