cancel
Showing results for 
Search instead for 
Did you mean: 

Motor control news from STMicroelectronics - Jan 2014

Gigi
ST Employee
Posted on January 23, 2014 at 16:00

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=22&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

http://links.st-microelectronics.mkt5947.com/ctt?kn=4&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

ST�s motor control software development kit provides all you need for the development of your motor control application based on the STM32 F0, F1, F2, F4 and now F3 (release v3.4) MCUs. It supports up to two PMSMs using any combination of current reading topologies and speed/position sensors, including sensorless operation. Application development and optimization is facilitated by the PC based MC Workbench software. This GUI sets SDK parameters, real-time access to control variables including their display on a virtual oscilloscope.

http://links.st-microelectronics.mkt5947.com/ctt?kn=25&ms=ODE3MTc2NQS2&r=NjkwODIyOTc4NjES1&b=3&j=MTk4Nzk3OTQzS0&mt=1&rt=0

Gigi

#stsw-stm32100-pmsm-foc-sdk
12 REPLIES 12
Gigi
ST Employee
Posted on December 12, 2014 at 13:59

Ciao

We are trying to simplify the download of the web distribution avoiding registration.

Anyhow you can get only the last version and so the v4.0 (up to now). Download the older version like v3.3 is non possible.

Ciao

Gigi

hassanbhutta91
Associate II
Posted on December 12, 2014 at 17:11

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards