cancel
Showing results for 
Search instead for 
Did you mean: 

MC workbench problem when project generation

FHuan
Associate

Hi ST ,

I use MC workbenck 5.2 to build a motor control project.

I select example project "STM32303E-EVAL-IHM045V1-Shinano-DUAL-DRIVE".

Use project generation function to build Keil MDK project, and everything is OK,

BUT, after modify some parameters, click generation->Update, and the MC workbenck program is halted like attached picture.

how to fix this problem ??

(i use single motor project ,"NUCLEO-F303RE-IPM10B-Shinano" , generate and update function is OK, only when i use dual motor project , always have update problem.... )

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards