2022-10-25 12:17 AM
MCU used: STM32F302C8T6
Program used: ST Motor Control SDK 5.4.8
Currently, we are using a compressor application for freezers, and it is a product with a built-in BLDC motor in the compressor.
There is one problem, but sometimes a step-out occurs. (That is, the operating frequency of the motor is recognized as normal, but the actual motor does not operate.) In this case, an overcurrent error does not occur. I'm trying to detect this manually. I am curious as to how it can be detected, so please reply after checking it out.
2022-12-06 2:47 AM
Dear Customer,
Can i have more information about your setup, do you use an encoder or hall sensors for your application ?
Thanks and best regards,
2022-12-06 4:19 AM
Hello.
Hall sensors or encoders are not used. I am using sensorless method(Observer+PLL). ST MOTOR CONTROL SDK 5.2 was used, and the configuration file (.SMTP) will be sent to you if you reply with your email address. thank you
2022-12-06 5:04 AM
Hello,
can you try it with MCSDK 5.4.8 or 5.Y.4 ?
which power board is used ?
I don't know what is the SMTP file can you send me your .stmcx file please ?
You can attach files here on the forum.
Thanks and best regards.
2022-12-06 5:15 AM