STM32 MCUs Motor control

Discuss STM32 solutions for motor control, including PID tuning, sensorless operation, ADC noise, custom algorithms, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

User Manual MCSDK documentation

  Dear MCSDK users, The full MCSDK documentation is embedded in the Motor Control Workbench tool. Refer to Workbench tool > About > Documentations > Documentation.This document provides: Introduction: Includes startup guide links for MCSDK, HSO featu...

GMA by ST Employee
  • 1763 Views
  • 0 replies
  • 0 kudos

MCSDK 6.4.0 is out!

Dear MCSDK users, MCSDK version 6.4.0 is now available: Download It here. This version of the new Motor Control SDK 6 series (X-CUBE-MCDSK) provides mainly FOC and 6Step improvements, here are the main changes for this version: Motor Control Features...

GMA by ST Employee
  • 4916 Views
  • 0 replies
  • 3 kudos

Board Manager documentation is out !

The documentation of the Board descriptions format is now available on Motor Control Boards Description Wiki page, this documentation is compatible with MCSDK versions from 6.1.2. Board Descriptions are used by the ST motor-control workbench to enabl...

Zied b. by ST Employee
  • 9645 Views
  • 5 replies
  • 3 kudos

Resolved! About MC Workbench DAC Functionality subblock

HiI m currently implementing a project using  MC Workbench software. There is a DAC Functionality subblock in the COntrol Unit block.  Can you tell me what is this block and why it uses two mcu pins as DAC ? For users which designing a custom board, ...

Capture.PNG Capture2.PNG
qqwq.1 by Associate II
  • 1486 Views
  • 1 replies
  • 0 kudos

Resolved! To Run & Stop A Stepper Motor

Hello, I'm using Blue Pill Board With TMC2209 Stepper Driver To Control 3 Stepper motors. I've made a project using Arduino Mega and there were MobaTools & TMCStepper libraries available to Set Current and run multiple motors at once smoothly.  I wan...

Increase current at startup

[VERSION]: MCSDK 6.2.1[TOOL]: MC Firmware.[DETAILS]:I developed a control/power board, a custom Hall sensors board and a motor (which will interface a reduction drive) for AGV application. I am using a dynamometer (link below) to measure maximum torq...

pzt by Associate III
  • 1756 Views
  • 0 replies
  • 0 kudos

Motor Control Protocol over USB CDC

Hi,I'm working on a project for an SM-PMSM motor drive. The end customer would only like communication via USB (with a micro connector).Is there a possibility to implement MCP and ASPEP protocols on the USB port instead of a UART?Has someone already ...

AlPo by Associate
  • 1002 Views
  • 0 replies
  • 0 kudos

Resolved! Using MCSDK API

Hardware:B_G473E_ZEST1S - Control boardSTEVAL-LVLP01 - Power boardMOONS R57BLB50L2 BLDC motorSoftware:MCSDK 6.2.1Code framework generated by MotorControl Workbench v6.2.1IDE STM32CubeIDECode customized only in main.c.  See attached.I was able to get ...

ccut93 by Associate III
  • 4632 Views
  • 2 replies
  • 0 kudos

Motor Control Workbench

Hello guys, I want to control an AC servo motor (ELM2H-0400LA60F) and a Motor Driver (RS-400P) with an STM32f407 discovery kit. But I cannot find my motor and control in the MC Workbench. Is it possible to work with MC Workbench in this regard?? 

STM32F407 Using GPIO to generate 5V PWM

I am working on the STM32F407 and we made some bad choises when selecting a motor. The motor control signal is 5V hence we need to generate 5V PWM signal using the STM32F407. Sadly, we have wired the GPIO from the STM32F407 directly to the motor cont...

LPetr1_0-1707223802637.png LPetr1_0-1707224113013.png LPetr1_0-1707225389413.png LPetr1_1-1707225618823.png
LPetr.1 by Senior II
  • 6109 Views
  • 4 replies
  • 7 kudos