cancel
Showing results for 
Search instead for 
Did you mean: 

IAR embedded WB from CubeMX to drive IHM003 motor control dev kit error : Error[Li016]: size limit exceeded. The application needs 0x86b6 (34'486) bytes

AGuze.1
Associate

When I run code in IAR embedded WB from CubeMX to drive IHM003 motor control dev kit initial project (same as in getting started video) , I have got this error

Error[Li016]: size limit exceeded. The application needs 0x86b6 (34'486) bytes, which is greater than the limit of 0x8000 (32'768) bytes.

           The limit is due to license "ARM.EW.LINKER" from "bus_voltage_sensor.o" (and 61 other modules).

I choose kickstart license due to other is paid and 30days for free.

If I turn to 30days trial everything is working normally.

Could you please help me on what is wrong with this?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Yes, you're right. I should have mentioned it.

A free alternative to IAR EWARM is STM32CubeIDE, available on st.com: https://www.st.com/en/development-tools/stm32cubeide.html

Regards

Fred V.

View solution in original post

3 REPLIES 3
Fred V.
ST Employee

Hello,

The issue you are facing is related to the licensing model of IAR EWARM.

The kickstart license is unlimited in time but is limited by the size of the resulting binary is can produce: 32 KBytes. If you need to produce bigger binaries as it is the case for the case you mention, you need the paid license (free for 30 days).

Regards,

Fred V.

> If you need to produce bigger binaries as it is the case for the case you mention, you need the paid license (free for 30 days).

It should be said that the cost of a full IAR WB licence is in the 4 digit range ($/€).

If you are not prepared to invest that, change over to a free IDE.

Yes, you're right. I should have mentioned it.

A free alternative to IAR EWARM is STM32CubeIDE, available on st.com: https://www.st.com/en/development-tools/stm32cubeide.html

Regards

Fred V.