cancel
Showing results for 
Search instead for 
Did you mean: 

I loaded the demo project from the workbench onto my STEVAL-SPIN3204, but whenever I use the monitor to start the motor I hear a beep and feel a pulse, but the motor does not spin. Did I miss anything?

MBale.1
Associate II
 
2 REPLIES 2
Laurent Ca...
Lead II

Dear @MBale.1​ 

Can we have a screenshot of the Motor Pilot Window?

Best regards

MBale.1
Associate II

This is the monitor from the legacy workbench. Whenever I try to set a speed and press "Start Motor", it immediately drops to 0. Also, the status is permanently set to "stop".0693W00000HqHDxQAN.pngThis image is of the motor pilot v 5.Y.30693W00000HqHE2QAN.png