cancel
Showing results for 
Search instead for 
Did you mean: 

Changing MCSDK6 config overwrites CubeMX configurations

Junde
Senior III

Hi there,

I am newbie to motor control, and I am studing how to use the excellent tool named MCSDK6.

Below is my work follows(MCU is STSPIN32G4):

1. open MCSDK6 and select my custom board and motor, generate the project;

2. open cubeMx configurate the others PINs, then generate the project;

3. write some app code;

4. i find the motor config is something wrong, so I open MCSDK6, change the config and generate the project again;

5. then I found the config in step2 is lost.

Is anything I did wrong? I think if the config could keep is better.

Thanks for you help.

1 REPLY 1
Gael A
ST Employee

Hello Junde,

Thank you for your post. I am sorry to inform you that this is an absolutely normal behaviour and that it can be listed as one of the limitations of our tool. When generating a Motor Control project, the WorkBench always create the .ioc file from scratch and thus any CubeMX modification is overwritten. However, user code is maintained after CubeMX generation as long as the code is located in the User Code brackets.
Thank you for your understanding.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.