2020-05-15 11:27 AM
Hi,
I have to make low cost on BLDC for Industrial Sewing Machine with Three Hall Sensors and read about BLDC from resources available on internet .
I have P-NUCLEO-IHM001 for BLDC motor control
and seen below youtube video from ST.
https://www.youtube.com/watch?v=h3ZuM2Z0UGs
It's based on IAR workbench.
How to Start: ?
1) How to start with BLDC motor control application with STM32CubeIDE,CubeMX
with ST Motor profiler with P-NUCLEO-IHM001?
2) Is it possible to generate code for FOC or BLDC with Sensors (Hall) , Six Step Commutation etc. with Software Tool Chain ?
3) How to connect Customized Hardware MCU and Drive (MOSFET) board the STMotorProfiler?
4) As this board can operate motor the max rating of 1.4 A RMS. How to design hardware
driver circuit for with Six MOSFETs and Driver circuit compatible the Software Tool Chain ?
Any other suggestions ..
Thanks in Advance ..
--
Karan
--
Karan
2020-05-19 9:27 AM
Hello Karan,
For your 3 first questions:
1/ Please use the MCSDK: https://www.st.com/en/embedded-software/x-cube-mcsdk.html
2/ Sensored FOC only is available for your slected board inside the MCSDK (not Six Step)
3/ Sorry the STMotorProfiler works only with ST boards so far...
Best regards,
Claire
2020-05-19 11:56 AM
Hi,
Thanks ..@ Claire OKU (ST Employee)
1) Will this board able to generate PWMs for Control operation of MOSFET for BLDC ?
2) How hall sensors are connected to this STM32 MCU?
https://www.st.com/en/embedded-software/x-cube-mcsdk.html
Thanks ..
--
Karan
2020-10-14 9:41 AM
Dear @Community member
Do you have still these problems to solve?
Best regards
Laurent Ca...
2020-10-14 11:06 PM
Thanks...
Not Yet..
--
Karan
2020-10-15 12:58 AM
Dear @Community member
Therefore I consider this thread closed.
If need, feel free to reopen it by posting a new answer.
Best regards
Laurent Ca...
2021-04-07 9:13 PM
Hi,
Thanks.. Can I reopen now ? If yes ..
Please consider as below:
I have to make low cost on BLDC FAN without any Sensors and first rotate/spin BLDC Motor (70-110 VDC) then control speed of motor for Ceilling Fan Application ..
I already have P-NUCLEO-IHM001 board for 12V BLDC .
I have decided to buy (NRND Product ) for this application.
https://www.st.com/en/evaluation-tools/steval-ihm040v1.html
Because I want to use STM32F100C6T6B and STGIPN3H60 in my application.
In this STEVAL-IHM040V1 hardware description Page 14 I have read "The BEMF sensing is not used by the FOC software".
Where Can I find demo code for that STSW-STM32100 ?
Can I use X-CUBE-MCSDK for generating Code of FOC to Rotate/SPIN the motor?
Any other suggestions are highly appreciated ...
--
Karan
2021-04-08 1:06 AM
Here is motor BLDC Motor Data:
110V DC , 32Watt , RPM 1350 Approx...
2021-04-08 10:53 AM
Hi,
I have also explored STEVAL-IHM038V1 (Active) for this application.
https://www.st.com/en/evaluation-tools/steval-ihm038v1.html
Where I can download demo code STSW-STM32100 (NRND) for that ?
--
Karan
2021-04-27 8:22 AM