2023-04-24 01:31 AM
follow the quick-start, i can set three shunt to active BR2804-1700kV.
but when i use single shunt, it always occured overload current.
when i set single shunt, i set the settting as the appendix
2023-09-06 06:14 AM
Hello hchin.1,
First of all, we would like to apologize for the delay in replying to your post.
If your point is still relevant, I would like to ask you if you have moved the jumper related to 1-Shunt configurations on the IHM07. They normally are set on 3-Shunt configuration, this may be the issue you are facing.