cancel
Showing results for 
Search instead for 
Did you mean: 

How to Measure Rs, Ls, BEMF Constant, and Max RPM of a PMSM Motor for STM32 FOC Tuning

Vedant07
Associate II

Hi all,

I'm working with an STM32-based motor control setup ( The EVSPIN32F0251S1 board is a 3-phase complete inverter based on the STSPIN32F0251 controller), and I have a physical PMSM motor that I want to use with FOC (Field Oriented Control).

I need help figuring out the following motor parameters:

Parameters I want to find:

Stator resistance (Rs in Ohms)

Stator inductance (Ls in mH)

Back-EMF constant (in Vrms/kRPM or Vpeak/kRPM)

Maximum mechanical RPM

What I have:

Physical motor only and basic data (no datasheet)

PMSM motor

Volt -24

Current -4.3 amp

Power -105W

RPM - 500 Hz- 83.3 Hz

Pole Pair -10

Torque -2.0 Nm

Can measure with multimeter, oscilloscope, etc.

Using STM32 Nucleo-F446RE board Planning to use STM32 Motor Control Workbench & SDK

My questions: What is the best method to measure Rs and Ls accurately with basic lab equipment?

How can I measure or estimate the BEMF constant?

Is there a reliable way to determine the maximum safe RPM if the motor model is unknown?

Can the STM32 MC Workbench help extract these automatically?

Any guidance, measurement techniques, or scripts/tools would be much appreciated!

 

Thanks in advance!

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Vedant07;

You can use MC Motor profiler tool provided on MCSDK available here. Feature is available using Nucleo-F446RE board.

You can also have a look to How To manually configure the motor parameters link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

1 REPLY 1
GMA
ST Employee

Hello @Vedant07;

You can use MC Motor profiler tool provided on MCSDK available here. Feature is available using Nucleo-F446RE board.

You can also have a look to How To manually configure the motor parameters link.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA