2023-03-30 03:07 AM
I have generated STM32CubeMX and STM32CubeIDE projects with the help of MC SDK.Referring to user manual, I connected the board to PC with USB and didn't use ST-LINK (I wonder whether it's OK). I don't know how to download the MC program to the board.
I also tried to control the motor with MC SDK monitor but I cannot connect the device,it indicated that "Connection failed, No response, check the communication cable, the power on the board or the baudrate (set to 9600 bps)" , though I did what it said.I feel so confused.
Best regards.
Thanks.
2023-09-06 06:57 AM
Hello Curve Wrecker,
First of all, I would like to apologize for the delay in replying to your post.
If your point is still relevant, I am wondering how you generated a project with an STEVAL-SPIN3204, as it is currently not supported by the Workbench. It is always possible to work from the STEVAL-SPIN3202 or to define the STEVAL-SPIN3204 thanks to the board manager but it is impossible to generate as is.
Concerning the general approach of the MCSDK, I encourage you to watch this video : https://www.youtube.com/watch?v=iTnj0DT3lBM