cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect X-NUCLEO-IHM08M1 with NUCLEO-H563ZI?

yang2
Associate III

Hello All

Does anyone know how to connect X-NUCLEO-IHM08M1 with NUCLEO-H563ZI?

I would to evaluate it with MC workbench 6.0.3.  However. I am not sure how to connect it together.

It looks like I CAN'T plug it directly, because the slot and pins are not matched.

yang2_0-1723707803038.pngyang2_1-1723707839085.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Gael A
ST Employee

Hello yang2,

As you said, X-NUCLEO-IHM08M1 and NUCLEO-H563ZI can't directly be plugged together, you need to solder pins on the CN11 and CN12 connectors of the NUCLEO-H563ZI to do so. H563ZI CN11 goes with IHM08 CN7, and H563ZI CN12 goes with IHM08 CN10. Be careful to keep the pins in the right order (Number 1 pin on number 1...) The first two pin numbers are written next to their respective connector for each board.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.

View solution in original post

1 REPLY 1
Gael A
ST Employee

Hello yang2,

As you said, X-NUCLEO-IHM08M1 and NUCLEO-H563ZI can't directly be plugged together, you need to solder pins on the CN11 and CN12 connectors of the NUCLEO-H563ZI to do so. H563ZI CN11 goes with IHM08 CN7, and H563ZI CN12 goes with IHM08 CN10. Be careful to keep the pins in the right order (Number 1 pin on number 1...) The first two pin numbers are written next to their respective connector for each board.

If you agree with my answer, please consider accepting it by clicking on 'Accept as solution'.

Hope this will help,
Gaël A.