How can change the RPM using motor control SDK API.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-14 1:36 PM
Hi,
SETUP:
IPM30B-3sh + STM32F302R8 + 2.5KW BLDC Motor
I have been trying to run the motor sensorless + PLL, i have been able to run the motor with predefined ramp.
question:
Q1. How can control the speed of motor using the gui tool and knob in MC-Workbench?
Issue:
Stops after the 5th ramp in advanced settings in parameter with a startup failure.
same issue with basic settings.
tried:
calling the motor control function i (defined in mc_api.c and mc_config.c), "StartMotor" & "MC_ProgramSpeedRampMotor1" inside main loop.
i want it to the motor to run continuously after the initial ramp-up stage till i hit or call StopMotor().
thanks,
Any help is appreciated.
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-05-25 1:18 AM
Dear @Tido
Welcome to the STM32 Community
Could you give more details to the STM32 Community about your setup -the material you use- including SW tools?
(HW and SW, CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM MC tools (such as MC_suite, MC-Motor Profile, MC-SDK, MC-workbench, and so on)?
Best regards
Laurent Ca...