cancel
Showing results for 
Search instead for 
Did you mean: 

power supply on evlservo1 control board

Lukas47
Associate II

Hello,

Is there a way to power the control board of the EVLSERVO1 without using the power board? I would like to just play around with the MCU before connecting to 48V for motor control. The ST-LINK V3SET does not provide any power to the board. 

Br,

Lukas

1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @Lukas47,

Refer to Evlservo1 User Manual "Figure 6. SERVO_CTRL1 board schematic (2 of 4): regulators" part and Stspin32g4 buck converter application note for more DC supply details.
On the current board design, VM provided through CON1/3 input is necessary.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

1 REPLY 1
GMA
ST Employee

Hello @Lukas47,

Refer to Evlservo1 User Manual "Figure 6. SERVO_CTRL1 board schematic (2 of 4): regulators" part and Stspin32g4 buck converter application note for more DC supply details.
On the current board design, VM provided through CON1/3 input is necessary.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA