2020-04-20 7:07 AM
If I select a SM32F303CB I can select "shared resources for both motors" using ADC1/2 for both motors. I don't understand why it works for the STM32F303CB and not for the STM32G474CBU.
Because of space and simple layout I want to use a STM32 in a UFQFPN48 case for two motors and 3-shunt measurement and Encoders.
It would be nice if someone can give me answer to my problem.
Best Regards,
Ulf
2021-06-27 10:33 PM
Adding of the "SM32 Motor Control" topic.
Best regards.