2020-03-27 1:04 AM
I need to use another mcu to link the motor control which use UART, But i can not find MCSDK 5.4.3 protocol, UM1052 is not the suggest document by ST.
2020-04-21 1:31 AM
Sorry, I'm not shure. But I think protocoll was part of old MCSDK docmentation. You can check e.g. MCSDK 4.3 docmentation.
2020-04-26 6:40 PM
Thanks your support, I have found by source code.
2020-04-29 9:57 AM
Can you share source code location? This could help others here.
2021-06-27 10:32 PM
The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards