cancel
Showing results for 
Search instead for 
Did you mean: 

Hello, I'm reading the application note PDF AN2388 for induction motor control algorithm. Is available somewhere the full code to download? Is it available any other detail on the implementation of IFOC on ST microcontroller?

AndreaC1985
Associate II
1 ACCEPTED SOLUTION

Accepted Solutions
Laurent Ca...
Lead II

Dear @AndreaC1985​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards

View solution in original post

1 REPLY 1
Laurent Ca...
Lead II

Dear @AndreaC1985​ 

There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.

Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .

Best regards