cancel
Showing results for 
Search instead for 
Did you mean: 

FOC control of 2 motors

RoyStevens
Associate III

I am currently working with a STM32G431RB and X-Nucleo-IHM08M1 and a motor with Halls. I want to drive 2 motors independently with the control board. Workbench seems to allow for 2 motors with FOC but not with the STM32G431RB.

In fact, there appears to be no combination of control boards and power boards which allow me to generate a project from Workbench 6.2.1 for 2 motors with FOC. 

Could someone please give me some advice on how to do this

Thanks

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
GMA
ST Employee

Hello @RoyStevens,

For STM32G474E‑EVAL board setup, power boards with "motor control connector" as STEVAL-IPMxx, have to be used.
Inverter boards are all in one setup (control + power) in the same hardware.

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

View solution in original post

3 REPLIES 3
GMA
ST Employee

Hello @RoyStevens,

For modular type boards, STEVAL-IHM039V1, STM32303E-EVAL and STM32G474E‑EVAL are dual drive capable.
Selecting "2 motors" on Workbench "General Info" tab and Inverter, Dual drive capable inverter boards are displayed.

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA

Thank you for the reply @GMAGMA.   I have selected STM32G474E‑EVAL and X-Nucleo-IHM08M1. There are no bridges available for this combination and when I select the other inverter boards you suggest there are no bridges available on the bridge selector tab in work bench. There is a button " click here to manage adapter devices" which brings up the STMC board manager and a bridge, but I do not know how to make these available to workbench. Some advice would be appreciated - thanks.

GMA
ST Employee

Hello @RoyStevens,

For STM32G474E‑EVAL board setup, power boards with "motor control connector" as STEVAL-IPMxx, have to be used.
Inverter boards are all in one setup (control + power) in the same hardware.

 

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA