2023-10-17 7:43 AM
Hello, I have a problem with running code, generated by motor workbench:
Guess it is not hardware problem, because i can run another project on it.
Error in final launch sequence:
Failed to execute MI command:
load C:\\Users\\tomek\\OneDrive\\Dokumenty\\st_workbench\\pls\\STM32CubeIDE\\Debug\\pls.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\tomek\\OneDrive\\Dokumenty\\st_workbench\\pls\\STM32CubeIDE\\Debug\\pls.elf
Error message from debugger back end:
Error finishing flash operation
Failed to execute MI command:
load C:\\Users\\tomek\\OneDrive\\Dokumenty\\st_workbench\\pls\\STM32CubeIDE\\Debug\\pls.elf
Error message from debugger back end:
Error finishing flash operation
Error finishing flash operation
Please help me :)
2023-11-07 8:19 AM
hai friend i am also having the same issue with stm32f411vet6 discovery board
did you got any solution
2023-11-07 8:57 AM
Could you describe your HW config ?
Did you try to flash your board with cubeProgrammer ?
Do you have an issue with Motor control generated code ? With a discovery board ? that sounds strange to me !
Regards
Cedric
2023-11-07 10:14 AM
Maybe you messed up the debugger settings. You can try to create a new debug configuration (Run => Debug Configurations => Right Click on STM32 C/C++ Application => New Configuration => Hit Debug button). It will be a clean default configuration. If it works, delete the old one.