2024-09-26 7:07 AM
Hello,
I am very new for ST MCU,I have made may own evspin32f0602s1 board , after many trial and errors also after gone through documentation ,I got PWM output. but problem is that I getting it at Reserved pins of MCU (TP1,TP2,TP3 in evolution board) .I have spend so much time but not getting any solution ,Please guide
Solved! Go to Solution.
2024-09-27 4:17 AM
"PWM idle state high side" and "PWM idle state low side", I just tried it ,
Nothing happens ,I tried with changed state also but no outputs are getting yet. hardware is ok sir, at least it should generate pulses
2024-09-27 4:31 AM
one point i am not getting that ,why I getting the output at Test points 1,2,3 ,instead of actual pins
2024-10-01 11:19 PM
Heelo sir, Atleast tell me what is the problem of driving ACIM through this board ,If we bypass BEMF then what will happens? my specific application is starting induction motor .it should rotate at 2880 / 1440 RPM and protecting IGBT in condition of short circuit and overload .
waiting for your valuable reply
2024-10-03 10:28 AM
why you people are not replying ,I need proper answer of my question that why we can't use this board for ACIM .if you cannot reply or if not give the proper solution then how could we use your hardware for our production.its not good thing
2024-10-04 3:35 AM
Hello KVijay32,
Let me summarize all the information :
- There is theoretically nothing that prevents you from running the ACIM algorithm on the EVSPIN32F0602S1, but this has not been (and will not be) tested on our end and therefore we cannot provide support on neither implementation nor configuration of the board.
- Using a custom hardware (despite being based on EVSPIN32F0602S1) is making hardware validation too complicated for us to provide support. As I already told you, your FW configuration should be able to output PWM, there is nothing more I can do for you.
2024-10-04 4:10 AM
its ok, i will try on my own ,i have that much confidence ,i can do this