cancel
Showing results for 
Search instead for 
Did you mean: 

EVSPIN32F0601S3 + ST Motor Profiler

SLodo.1
Associate

Hey. When will it be possible to add the EVSPIN32F0601S3 board to the ST Motor Profiler? Or which one to choose from the proposed for determining the parameters of the electric motor?

1 ACCEPTED SOLUTION

Accepted Solutions
Enrico Poli
ST Employee

Hi @SLodo.1​ , unfortunately the EVSPIN32F0601S3  is not supported by the motor profiler.

However you can collect the motor characteristics using the STEVAL-IPM05F as power board.

View solution in original post

4 REPLIES 4
Enrico Poli
ST Employee

Hi @SLodo.1​ , unfortunately the EVSPIN32F0601S3  is not supported by the motor profiler.

However you can collect the motor characteristics using the STEVAL-IPM05F as power board.

Karan 123
Senior

Hi @Enrico Poli (ST Employee) , SLodo.1 (Community Member)

Which combination should I use for EVSPIN32F0601S3 in Motor Profiler 5.4.6?

0693W00000ANtnEQAT.png 

How the hardware ( Nucleo Board + STEVAL-IPM05F) will be identical/matched with EVSPIN32F0601S3 to Run Motor Profiler ?

or you suggest buy another board?

Thanks in advance ..

--

Karan

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Any pair of equipment can be used (also in conjunction with nucleo 103). The choice of power section depends on the capacity and power supply of your drive. Then you can use EVSPIN32F0601S3 to mcwb to create a project with parameters from Motor Profiler.