cancel
Showing results for 
Search instead for 
Did you mean: 

STM32C092FCP6 FDCAN remapping issue.

JennyDigital
Associate II

I designed a board with a layout that I was very happy with, but this meant remapping FDCAN1_TX to PC14, which CubeMX dutifully created code for...

However, the code wouldn't compile.  I needed to get my board order in that day so I simply adjusted the pin arrangement and modified the layout, but it looks for all the world as though there are some missing defines.  I say this because the datasheet quite clearly states this as a valid remapping.

Just thought I'd put this out there.

Maybe the fix is as simple as:-

#define GPIO_AF13_FDCAN1 13

I may revisit this in the near future and I am aware there are some other remapping issues others have tripped up on.  I guess it's because this is a relatively new part.  It only came out in Feb 2025.

Does anybody else know anything about this issue?

0 REPLIES 0