2024-10-10 07:43 AM - edited 2024-10-10 07:54 AM
I connected the B-G431-ESC inverter to a DJI2312 motor and created the project on MC Workbench version 6.1.0 (I also tried 6.1.3).
I would like to use the motor pilot but when I press on "discover board" the board is not recognized.
In the generated the IDE .c file and a baudrate = 115200 is specified in "MX_USART2_UART_Init "
What is the orange mesage?
I updated ST-LINK with the last version using STM32 ST-LINK Utility