2019-07-24 02:56 AM
i have generated code from motor control workbench and when i build this code the error came as,
region `FLASH' overflowed by 18000 bytes StSpin_Hall_24_07 C/C++ Problem
StSpin_Hall_24_07.elf section `.text' will not fit in region `FLASH' StSpin_Hall_24_07 C/C++ Problem
i tried for optimised the code code then the there is no error but motor is not working well.......
2021-06-22 01:21 AM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards