Doing 6-step using FOC algorithm
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-03-03 1:00 AM
Hello,
I've generated a functional FOC project, with speed encoder. I also have Hall sensors wired (only used for my 6-step mode).
I'd like to implement a basic 6-step control mode in this project.
The FOC code allows me to set (eg. during the encoder alignment phase, hacking it) the IqdRef values.
I thought that I could control the orientation of the magnetic field to place it in each of the six sectors like so:
switch (sector_step) {
case 1:
IqdRef.q = cos(0°) * magnitude;
IqdRef.d = sin(0°) * magnitude;
break;
case 2:
IqdRef.q = cos(60°) * magnitude;
IqdRef.d = sin(60°) * magnitude;
break;
case 3:
IqdRef.q = cos(120°) * magnitude;
IqdRef.d = sin(120°) * magnitude;
break;
And so on...
But this does not behaves as expected (weak torque, torque weaker in one direction... despite correct Hall alignment and position confirmed on oscilloscope).
Is this logic correct ?
Can I do basic 6-step control like this by controlling the IqdRef currents ?
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-09-20 6:25 AM
hello @Quentin Ch ,
Hello, we already offer in our MCSDK a solution that works with 6-step, trying to do 6-step with a Foc algo does not seem relevant to me. If you need help using our 6 step algo, don't hesitate to look at the MCSDK documentation or ask a new question on the forum.
regards