cancel
Showing results for 
Search instead for 
Did you mean: 

Does the STEVAL-CTM010V1 support 115200 baudrate ?

wcx8229
Associate II

Hello,

      I use MCWB 6.4.0 & Motor Pilot 6.4.0, STLINK V3 MINIE.

      Motor Pilot can not discover STEVAL-CTM010V1 board.

      And  I find that MCU can receive datas at buadrate 1200 to 14400, but failed at 19200  or  more fast .

      Does the STEVAL-CTM010V1 support 115200 baudrate ?  Or PC817B doesn't  support this baudrate?

 

      this issue seems like this one, https://community.st.com/t5/stm32-mcus-motor-control/steval-ctm010v1-board-can-not-work/m-p/241708#M4301 

2 REPLIES 2
wcx8229
Associate II

so is steval-ctm010v1 board , even if  exist some years,  a mature solution ?

Hello @wcx8229,

According to this post, you are able to connect the MC Pilot with your board. Could you share what was the issue root cause?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA