Skip to main content
Associate II
June 19, 2025
Question

How to modify the BUS VOLTAGE ?

  • June 19, 2025
  • 4 replies
  • 897 views

Hello,

Why is the bus voltage remain  about 330v when motor max-voltage is changed to 280v ?

the attchment is the status of Motor Pilot based on STEVAL-CTM010V1 .

BUS VOLTAGE 330V.png

This topic has been closed for replies.

4 replies

cedric H
ST Technical Moderator
June 19, 2025

Hello @wcx8229 

When Bus voltage sensing is enabled as it is your case for Motor 1, the value is read from the board and does not depend on the motor max-voltage.

How is your board powered?

Regards

Cedric

 

wcx8229Author
Associate II
June 20, 2025

Thanks for your support.

The power input is 220VAC 50HZ .

So could you tell me how can I get a 280v bus voltage ?

CTM010.jpg

 

wcx8229Author
Associate II
June 26, 2025

So steval_ctm0101v1 does not support 280V BLDC motor because of OVER VALTAGE ?

 

RobK1
Associate II
June 26, 2025

Just exactly how do you think this thing would be able to make a 280V bus voltage with a 220VAC input?