cancel
Showing results for 
Search instead for 
Did you mean: 

BiSS-C library/support for STM32H7A3ZIT6

Gowri123
Associate

 

Hello everyone,

I am new to STM32 development and I am working with the STM32H7A3ZIT6 microcontroller. I need to interface it with a BiSS-C encoder/sensor.

I would like to know:

  1. Is there any ready-made or full BiSS-C communication library available for STM32?

  2. Does STM32CubeMX / HAL provide any support for BiSS-C?

  3. If no full library is available, what is the recommended way to implement BiSS-C on STM32H7A3ZIT6?

  4. Can BiSS-C be implemented using SPI, timer, DMA, or GPIO bit-banging on this MCU?

Any example code, application note, or guidance would be very helpful.

Thank you.

1 REPLY 1
mƎALLEm
ST Employee

Hello,

https://community.st.com/t5/others-stm32-mcus-related/biss-c-implementation/td-p/81200

PS: to my knoweledge no ST library provided nor documentation assiociated to BiSS-C library.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.