cancel
Showing results for 
Search instead for 
Did you mean: 

Does ST MC Workbench allow room to improve motor control ?

CBald.1
Associate II

Hi everyone,

I am using a p-nucleo-ihm03 pack to try to improve the control of the motor included. The issue I am having is that if the software already performs FOC for you. Is there any room for the user to improve the control of the motor ? Please could you let me know the areas which could be improved by means of the Workbench or any other related tools you may know of ? Thanks in advanced.

P.S. Also could someone let me know if the Gimbal motor in the p-nucleo-ihm03 is a PMSM or a BLDC motor ? I have looked everywhere online but I haven't found the answer.

2 REPLIES 2
chaaalyy
Senior II

Even, if there´s no "standard" example available for this pack, in the description for X-CUBE-MCSDK, i found the promotion, source code is provided ...

But anyway: sometimes reality and expectations (especially, when working with ST´s stuff ;) ) differ ...

/Charly

Laurent Ca...
Lead II

The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards