Default st motor control project for SPIN3202 board doesn't compile.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 2:54 AM
Dear all,
im running into the problem that the compilation of a fresh generated project using the motor control workbench fails to compile for the SPIN3202 board.
In the default settings RAM and ROM is overflowed. When i set the opitmisation to speed or code size, the ROM isn't overflowed anymore but the RAM ist still overflowed by 8 Bytes.
section `._user_heap_stack' will not fit in region `RAM'
region `RAM' overflowed by 8 bytes
I generated the project according to https://my.st.com/content/ccc/resource/technical/document/user_manual/group0/d9/d1/b2/67/be/15/42/76/DM00361065/files/DM00361065.pdf/jcr:content/translations/en.DM00361065.pdf
I'm using the STM32CubeIDE with version 1.1.0 and haven't added any usercode yet.
Are there any options for me to test the default project on this hardware?
- Labels:
-
STM32 Motor Control
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-02-06 2:52 PM
Just found out that the generated program will barely fit into memory with full optimisation and a heap size of 0x00. I hope that disabling the uart control gives me enough space to write my own code on top of the basic project.
I also downloaded Keil and found out that the Keil compiler did a better job at generating code than the gcc and so the compiled code is smaller with the Keil IDE. Luckily the Keil MDK is free for STM32L0 G0 and F0.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-03-30 9:53 PM
I am having the same issue! I will try Keil. I hope it fixs the problem!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-06-21 11:00 PM
The question has been moved from the section "Motor Control Hardware" to the "STM32 Motor Control" section (the question is about the STM32 MC SDK).
Best regards