cancel
Showing results for 
Search instead for 
Did you mean: 

Current Measurement Discrepancy Between STDRIVE101 + NUCLEO F303RE and Custom Board with STM32F303VC

Christophe65
Associate III
Hello everyone,
I created a project using Motor Control Workbench, configured for FOC with Hall sensors and 3-shunt current sensing, PWM at 20 kHz. The initial setup used:
  • NUCLEO F303RE board
  • STDRIVE101 evaluation board
  • A BLDC motor with a nominal current of 4 A
During testing, everything worked perfectly: the current reading matched the expected load (4 A at constant effort).
Based on this setup, I developed a custom electronic board using an STM32F303VC. The schematic is identical to the EVALSTDRIVE101 board (same components).
I reconfigured the project in MC Workbench using exactly the same parameters as in the evaluation setup. However, when testing the custom board under the same load conditions, I read a current of 8 A.
I’ve double-checked the hardware: shunt resistor values, op-amps, connections — everything is identical. I suspect a configuration issue or a subtle difference I may have overlooked.
Questions:
  • Are there any specific parameters in MC Workbench or Motor Pilot that depend on the exact microcontroller model (RE vs VC)?
  • Could differences in ADC behavior or internal amplifier gain explain the doubled current reading?
  • Has anyone experienced similar issues when switching from ST evaluation boards to custom designs?
Thanks in advance for your help!
Christophe
3 REPLIES 3
GMA
ST Employee

Hello @Christophe65,

Are the workbench current sensing parameters (gain and shunt resistor) aligned between both projects?
Is the current scaling factor CURRENT_CONV_FACTOR_INV used by Motor Pilot identical?

If you agree with the answer, please accept it by clicking on 'Accept as solution'.
Best regards.
GMA
Hello @st_Community,
Yes, all current sensing parameters — including gain and shunt resistor values — are identical between both projects. I’ve already checked them multiple times, and I’m currently reviewing everything once again to be absolutely sure.
The value of CURRENT_CONV_FACTOR_INV used by Motor Pilot also appears to be the same, but I’ll re-verify it during this last check.
Thanks again for your support,
Christophe
federico.rodighiero87
Associate III

possible layout or circuit issue, post the schematic.

HW/FW Motor Control Engineer
https://www.linkedin.com/in/federicorodighiero/