2023-10-16 6:01 AM
Hello all,
I have an application in which I want to control four BLDC motors independently using the FOC. I want to use a STM32G484 for this. The question now is how I can distribute the interrups so cleverly that I can control all motors with 16kHz without them blocking each other.
Many thanks for your answers :)
Solved! Go to Solution.
2023-10-18 12:54 AM
hi @L_Kopp ,
I can also suggest you look at the B-G431-ESC card, it is possible to control it from a PWM input to vary the speed with the Electronic Speed Control, you can for example have 4 ESCs and one central control card.
here is information on how the ESC works:
The electronic speed control (ESC) feature allows to control the motor speed with a PWM signal in input, for example on the B-G431B-ESC1 boards it is possible to use this feature to control the motors of a drone sending a PWM signal with a different duty cycle to switch the motor to armed, armed with a minimum speed, armed with a maximum speed and unarmed state.
You can find more details on this example on this link : click here
2023-10-17 8:04 AM
Hi @L_Kopp
In the solution that we propose on the MCSDK, it is possible to use the STM32G474E-EVAL Board with 2 motors, but the current solution does not offer baords that make more than 2 motors. One of the ideas that I can suggest to you is to use 2 baords and have them communicate by Uart for example. Out of curiosity, can you tell me for which application you need 4 motors?
Regards
2023-10-17 10:31 PM
Hey @Zied b.
thank you for your answer. For a first try I can use two Nucleo boards but later I want to design my own board and use only one MCU if possible. Here, as I said, I'm not sure how to get the timings right so that all four motors can be controlled independently.
The application is a mobile robot :)
Regards
2023-10-18 12:54 AM
hi @L_Kopp ,
I can also suggest you look at the B-G431-ESC card, it is possible to control it from a PWM input to vary the speed with the Electronic Speed Control, you can for example have 4 ESCs and one central control card.
here is information on how the ESC works:
The electronic speed control (ESC) feature allows to control the motor speed with a PWM signal in input, for example on the B-G431B-ESC1 boards it is possible to use this feature to control the motors of a drone sending a PWM signal with a different duty cycle to switch the motor to armed, armed with a minimum speed, armed with a maximum speed and unarmed state.
You can find more details on this example on this link : click here
2025-03-15 3:01 AM - edited 2025-03-15 3:01 AM
Hello,
I am interested in usage of stm32g4 with x4 stdrive101 to control x4 BLDCs from single MCU with FOC.
My idea for design is to use:
- x3 advaced TIM's with break funktionality and x1 TIM without such to drive one stdrive101 each
- stdrive101 shall provide fixed pwm phase shift for H-bridge protection
- x4 ADC channles with x4 OPAMPs for current sensing on x1 shunt residtor. IMPORTANT: There is no way around one-shunt reistor on H-bridge, since number of OPAMPs is limited to max x8 on one stm32g4.
- x1 TEMP temperature sensor for over-temperature protection
- x1 VBUS sensor for bus voltage sensing
Please let me know, if you see some potential pitfalls NO-GO's in mentioned design idea.
Currently I am inspierd by https://www.st.com/en/evaluation-tools/steval-ptool4a.html#cad-resources steval-pool4a schematic design.