cancel
Showing results for 
Search instead for 
Did you mean: 

Connecting EVALSTDRIVE 101 and Nucleo F446RE

KoLL
Associate

I am planning to purchase a BLDC motor drive from ST. I have shortlisted EVALSTDRIVE 101 and Nucleo F446RE. There is a lack of clarity on how this two boards are connected together. Should I purchase X-Nucleo-IHM09M2 or something else

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @KoLL, to the community!

The UM2781, rev 1 mentions in section 2 that an X-NUCLEO-IHM09M1 can be used to connect NUCLEO and EVALSTDRIVE101. However, the X-NUCLEO-IHM09M1 has since been discontinued by NRND and replaced by the compatible successor X-NUCLEO-IHM09M2. Both interface boards are of course not absolutely necessary, but make it easier to connect the motor control boards via the 34-pin motor control connector.

The only other things you need are a 34 pole 1.27mm pitch flat cable, a USB cable for the NUCLEO, power supply and motor and, of course, a PC.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @KoLL, to the community!

The UM2781, rev 1 mentions in section 2 that an X-NUCLEO-IHM09M1 can be used to connect NUCLEO and EVALSTDRIVE101. However, the X-NUCLEO-IHM09M1 has since been discontinued by NRND and replaced by the compatible successor X-NUCLEO-IHM09M2. Both interface boards are of course not absolutely necessary, but make it easier to connect the motor control boards via the 34-pin motor control connector.

The only other things you need are a 34 pole 1.27mm pitch flat cable, a USB cable for the NUCLEO, power supply and motor and, of course, a PC.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.