cancel
Showing results for 
Search instead for 
Did you mean: 

Change  phase 120 degree to 90 degree in MotorControl Workbench 6.2.0?

methee_c
Associate III

Hi All ,

I need to change  phase 120 degree to 90 degree in MotorControl Workbench 6.2.0 

Can change in file mc_math.c?

For use single phase motor 3 wire  

Please help me for advice.

 

BR,

METHEE

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @methee_c 

I am not an ACIM expert but your motor sounds weird to me.

You mentioned single phase? three wires? and an angle of 90 degrees...

Do you have any commercial reference of your motor I can look at?

Regards

Cedric

 

View solution in original post

4 REPLIES 4
SRedd.5
Senior III

Do you use FOC (sensored / sensor less) , 6 step commutation? What you want to change in mc_math.c?

Hi SRedd.5,

I test run on ACIM open loop,I see  table and config in mc_math 

You can help me for Change  phase 120 degree to 90 degree in MotorControl Workbench 6.2.0?

BR,

METHEE

Hello @methee_c 

I am not an ACIM expert but your motor sounds weird to me.

You mentioned single phase? three wires? and an angle of 90 degrees...

Do you have any commercial reference of your motor I can look at?

Regards

Cedric

 

Hi cedric H,

 I changed  pole = 2  from looking at the machinery. normal current.

Thanks you,

Regards

Methee