cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot get motor parameters - ST Motor Pilot V1.2.12 - profiler

wickeLine228
Associate II

I am using GBM1008H-150T PMSM motor. Cannot get motor parameters using "Start profile". Motor is noisy and rotates jerkily. I am applying 24V. Specification says the motor has 14 pole pairs and 7 KV.
wickeLine228_0-1740135115619.png

wickeLine228_2-1740135153129.png

 

0 REPLIES 0