2021-09-16 02:03 AM
I have STM3210B-MCKIT PMSM starter control kit, It is worked through LCD and for start and stop the motor.
but I would like to develop a new controller and change the control system. I would like to a guide and If there is a library that has the projects for this starter kit?
how can I measure the currents with an oscilloscope through ADC, I can find these pins in the kit?
I asked after a spent a long time, so please help me!
2021-10-20 05:28 AM
Dear @ADiab.2
Welcome to the STM32 Community
Sorry for late answer.
Could you give more details to the STM32 Community about your setup -the material you use- ?
(HW and also SW: CPU(s), tools and versions, board(s), motor(s) and so on)
And more especially did you use STM32 MC tools (such as MC_suite, STM32 MC Motor Profile, STM32 MC SDK, STM32 MC Workbench, the used example, the origin of the base of your application source code, and so on)?
Best regards