cancel
Showing results for 
Search instead for 
Did you mean: 

Can ST Motor Control use absolute encoders?

Leonelf
Associate II

I'm developing a PMSM inverter for a motor that has a built in absolute encoder and I'd like to continue using this encoder instead of using sensorless or hall/quadrature schemes. Can I use the MC-SDK with a custom encoder (just feeding it with angle values)?

1 REPLY 1
Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards