Skip to main content
CPrin
Associate II
February 21, 2019
Question

Can I use the MC monitor with our custom board?

  • February 21, 2019
  • 5 replies
  • 1333 views

We have developed our own MC board, based on STM32F303 Nucleo-64 with some different pinout. We do not have integrated ST-LINK like the Nucleo board of course, just a JTAG connector. Can we use our custom board in combination with the MC monitor? When I press now the "connect" button, it does not connect. The code was generated correctly by MCWB, some additions made with STM32CubeMX, code generated for Keil v5 and flashed into the custom board. The software functions in our custom board, serial connection is available and we tested it with a simple terminal program.

This topic has been closed for replies.

5 replies

CPrin
CPrinAuthor
Associate II
February 21, 2019

In the meantime I succeeded in using our own MC board in combination with the MCWB :) very happy with it!

Liam G
Associate II
April 7, 2019

Hi Cojan. This is interesting and exactly what I want to do. How did you wire the 2 UART signals back to the PC? Through the JTAG in some way or using a separate RS232 to USB path with a COM port on the PC? Thank you.

CPrin
CPrinAuthor
Associate II
April 8, 2019

Hi Liam, I just used the "normal" USART and we have a FTDI FT230X connected between the USART and the PC. This works fine. We use USART1 with different pinout. The best way is to have it configured within the ST Motor Control Workbench, because it will be automatically shown correctly in STMCubeMX. Setting/changing the pinning in STMCubeMX sometimes seems not to be working correctly.

Liam G
Associate II
April 24, 2019

Thank you. This was very helpful.

Laurent Ca...
Senior III
June 28, 2021

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards