User Activity

I have the Shinano motor running correctly with the NUCLEO-F303RE board and the X-NUCLEO-IHM08M1. I'm trying now to get it working with our custom board. Unfortunately my hardware colleagues have used the NCP5304 bridge driver instead of the L6398 dr...
We have developed our own MC board, based on STM32F303 Nucleo-64 with some different pinout. We do not have integrated ST-LINK like the Nucleo board of course, just a JTAG connector. Can we use our custom board in combination with the MC monitor? Whe...
We have developed our own MC board, based on STM32F303RE (like the STM32F303 Nucleo-64 board). The pinout is slightly different. In the MCWB I can set the pinning correctly for the 3 phase but in what way can I set the correct ADC input to the B-EMF ...