2020-02-10 04:24 AM
2021-06-28 05:52 AM
Dear @RAyub.1
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards
2020-02-14 01:51 AM
Hello Rayub.1,
So far we don't have STM32 libraries to run induction motors. Sorry about this...
Thanks and best ergards,
Claire
2020-02-23 08:59 PM
Hello Rayub,
STEVAL-IHM028V2 is just a 2kW power stage without the controller. The power stage can support both three phase induction motors as well as three phase BLDC/PMSM motors.
For V/f control of three phase ACIM it is possible to use STM8S or STM8A MCU with STSW-STM8020 firmware library.
https://www.st.com/en/embedded-software/stsw-stm8020.html
Regards
2021-06-28 05:52 AM
Dear @RAyub.1
There is now in the last SDK version demonstration firmware example projects for ACIM showing how the STM32 MC SDK can be used to drive an asynchronous induction motor (ACIM) in field-oriented control (FOC) using a sensorless state observer algorithm to estimate the electrical and mechanical speed and position of the rotor and the rotor flux, or in V/F open-loop sensorless mode.
Please have a look on our STM32 Motor Control Knowledge database here: https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor .
Best regards