Skip to main content
Visitor II
June 17, 2023
Question

BLDC motor driver

  • June 17, 2023
  • 1 reply
  • 1610 views

Hello. I would like to design a bldc motor controller using stm32G4 series. I recently ordered stm32g431rbt6 because of the on chip opamps and dacs. Also in the datasheet it states that there are timers for advanced motor control. I am seeking assistance on where to start with the motor controller design and what tools from STM I can use to achieve my goal. The project has a limited deadline and I would like support on the controller design. The motor I will be using is a hub motor. I would also appreciate any other information concerning microcontroller selection and whether I should use a different microcontroller. Thanks.  

This topic has been closed for replies.

1 reply

RhSilicon
Lead
June 18, 2023