cancel
Showing results for 
Search instead for 
Did you mean: 

Looking for an ST-made inverter board with resolver/encoder interface for FOC-controlled PMSM

htuncer14
Associate

Hello,

I’m working on a FOC (Field Oriented Control) project to drive a PMSM (Permanent Magnet Synchronous Motor). I’m looking for an official STMicroelectronics development board that includes the following features:

  • STM32-based microcontroller

  • Supports resolver and encoder input (preferably both)

  • Gate driver outputs for external power stage (or integrated solution is fine)

  • Fully compatible with FOC-based motor control

Does ST offer such a motor control/inverter board?
Please recommend any official ST hardware that fits these criteria.

 

0 REPLIES 0