cancel
Showing results for 
Search instead for 
Did you mean: 

BLDC Drive for BLDC Ceiling Fan High Voltage:

Karan 123
Senior

Hi,

I have to make low cost on BLDC Drive for BLDC Ceiling Fan ( 110V ) without any sensors.

This topic is continuation from below thread as below thread don't pay much attention there as required :

https://community.st.com/s/question/0D73W000000Uy06/detail?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&s1uid=0050X000007vw7K&emtm=1602748687452&fromEmail=1&s1ext=0

Below are parameters which I have:

0693W00000ANImfQAH.png 

I have download below softwares :

https://www.st.com/content/st_com/en/products/embedded-software/mcu-mpu-embedded-software/stm32-embedded-software/stm32cube-expansion-packages/x-cube-mcsdk.html

0693W00000ANJBEQA5.png 

And seen below Eval-Board .

https://www.st.com/en/evaluation-tools/evspin32f0601s1.html

Please suggest . . .

How do I start ?

Many of Thanks in advance ..

--

Karan

14 REPLIES 14
Javier1
Principal

so you have the EVSPIN32F0601S1eval board with you?

Maybe you can show us your wiring in case nothing is blinking or you dont know where to start

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

Hi​,

Thanks for update..

I don't have ​EVSPIN32F0601S1eval board with me.

I have ​ P-NUCLEO-IHM001 board which is meant for LV application.

Meanwhile, I am trying to learn MC-SDK for EVSPIN32F0601S1eval according to motor specifications given at Msg#1.

​​

I​ will order that .

--

Karan​

@Community member​ just to clarify, i have never used ​EVSPIN32F0601S1eval , i was just answering your question >How do I start ? -buy the hardware first

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

Yes, I have ordered but not yet received . Which LV or HV Board you have used for BLDC ?

Ive used P-nucleo-IHM001 and it worked out of the box but its only for small motors.

Ive also tried unsuccesfully this board for bigger motors, but i ended up using custom hardware and opensource motor control software like vesc

https://community.st.com/s/question/0D50X0000BfvEqOSQU/is-anyone-trying-to-use-stevalipm15b-for-foc-motor-control

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

Hi,

Thanks for update ... Means you have successfully Implemented BLDC HV Drive ? 

1)

When I have EVSPIN32F0601S1eval board with me do I need only Enter Motor Parameters as in Msg#1 in mcsdk to spin the Motor ?

2)

Do I need to change Feedback resistance(s) in Board EVSPIN32F0601S1eval board .

What kind of other changes in mcsdk ..?

Any other suggestions..

--

Karan  

Please update. ​

@Community member​  if you dont tag me i dont get the notification (dont know why)

1) no idea, you should first run the motor profiler tool to get your parameters.

2) i dont know the board and i dont know what feedback resistors youre refering to.

Available for consulting/freelancing , hit me up in https://github.com/javiBajoCero

@Javier (Community Member)

 EVSPIN32F0601S1 or S3 is not supported my Motor profiler Tool Yet