cancel
Showing results for 
Search instead for 
Did you mean: 

Anybody from ST care to comment on when a reliable, working motor control SDK and firmware will be released? So many people having issues with V6, no documentation, bugs in the firmware, only half implemented and almost definitely not tested!

jartim
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hi Fred, sorry for the long delay in replying.

Here's how I found this optimisation issue -

1:Import the project into the IDE from the workbench generated code

2: Set the C/C++ Build / Settings / MCU GCC Compiler / Optimization / Optimization level to None (-O0)

3: In the IDE, load the IOC file and change something - add a peripheral, modify a GPIO line etc.

4: In the IDE, compile the IOC file.

5: Go back to C/C++ Build / Settings / MCU GCC Compiler / Optimization / Optimization level - the value has changed to Optimize for size (-Os)

Regards

Tim