cancel
Showing results for 
Search instead for 
Did you mean: 

ACIM support - which version to use?

lamare
Associate

On the wiki page:

https://wiki.st.com/stm32mcu/wiki/STM32MotorControl:SDK_AC_induction_motor 

It says:

""This article applies to the 5.Y.* versions series of the X-CUBE-MCSDK. ACIM motors are not supported in older versions of the X-CUBE-MCSDK (v5.4.* and before). They are not supported yet in X-CUBE-MCSDK versions 6.*."

 

However, the latest v5 version I can download is 5.4.8.

 

So, it appears that I would need to use version 6 to compile the examples, while full support comes later?

 

 

 

 

 

 

 

0 REPLIES 0