cancel
Showing results for 
Search instead for 
Did you mean: 

AC Servo Motor with STM32f407

tnishanthraj
Associate II

Hello guys, I'm looking to control an AC Servo motor with STM32f407- Discovery kit. There are a lot of resources for DC motor, but i couldnt find many for AC Servo. Can anyone suggest on how to approach or share me some resources? Thanks in advance.

4 REPLIES 4
cedric H
ST Employee

Hello @tnishanthraj ,

Do you have any reference of the motor you want to drive ?

Are you sure it is not a BLDC motor or a PMSM motor ?

Cedric

Yes, I'm using ELM2H-0400LA60F AC Servo Motor with EL7-RS400P Servo Drive.

Hello @tnishanthraj ,

If you use a EL7-RS400P Servo Drive, what is the purpose of the STM32F407 Discovery kit ?

Your motor seems to be a PMSM (Permanent Magnet Surface Mounted), and can be driven by FOC algorithm.

We provide a Motor Control SDK downloadable here. But as stated in the name, it is a development kit providing motor control FOC algorithms and API to allow you to develop a motor control application on top of it. 

Regards

Cedric

jealab
Associate

The control an AC Servo motor with the STM32f407 Discovery kit, start by understanding the motor's specifications and interface requirements. Implement a control algorithm, possibly using a Proportional-Integral-Derivative (PID) controller, tailored to the servo's characteristics. Leverage STM32's PWM capabilities for precise motor control.