cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-EEPROM 7.0.0 bug

pretoriandave
Associate II

While implementing EEPROM emulation on an STM32G0 (although I believe this would apply to all supported families) I have discovered what I believe to be a bug in eeprom_emul.c:

Although ConfigureCrc() is called at the beginning of EE_Init to turn on the CRC block clock, it is not similarly called at the beginning of EE_Format and I believe it should be.

The effect of this is that if you call EE_Format first to configure the EEPROM emulation pages and then write some values in, the CRCs are all written to zero. On subsequent power/reset cycles, when usign EE_Init, ConfigureCRC is called, allowing the CRCs to be caculated correct from there on, although subsequent reads using EE_ReadVariablexxbits fail due to bad CRC, since the stored CRCs are all zero.

Adding ConfigureCrc(); at the beginning of EE_Format fixes the issue.

EE_Status EE_Format(EE_Erase_type EraseType)
{
  uint32_t page = 0U;

  ConfigureCrc();	//***BUG FIX***										

  /* Check if the configuration is 128-bits bank or 2*64-bits bank */
  if (FI_CheckBankConfig() != EE_OK)
  {
    return EE_INVALID_BANK_CFG;
  }
etc

 

1 ACCEPTED SOLUTION

Accepted Solutions

@pretoriandave wrote:

Many thanks @mƎALLEm , great service as ever. I think there may be an important distinction in here that we should bottom out, as I think it might warrant a tweak to AN4898 and/or the headers in eeprom_emul.c as they seem to be at odds...

I think what I'm gathering from the team's response is that, despite the function name, EE_Format is not how one should first format the EEPROM emulation space. In any case, without my tweak, you can't, since the CRC block is not clocked.

The response above is that calling EE_Init is mandatory after each reset and I presume that includes the very first time the MCU is powered after programming too. In other words, one should use the following to first format the EEPROM space..

EE_Init(EE_FORCED_ERASE)

By contrast, the header of eeprom_emul.c says:

(#) EEPROM emulation initialization functions:
           (++) Format the FLASH pages used by EEPROM emulation using EE_Format().
                This function is optionally used, it can be called the very first
                time EEPROM emulation is used, to prepare FLASH pages for EEPROM
                emulation with empty EEPROM variables. It can also be called at
                any time, to flush all EEPROM variables.
           (++) Initialize EEPROM emulation, and restore the FLASH pages used by
                EEPROM emulation to a known good state in case of power loss
                using EE_Init(). It must be performed at system start up.

The header suggests that EE_Format can be used to format the EEPROM space the first time the MCU is powered and the function name certainly supports that view. That is how I first did it and it didn't work for the reasons already stated. 'It can be called the very first time EEPROM emulation is used'. No it can't.

My use-case is that I am storing calibration parameters in the EEPROM emulation space which are determined the very first time the MCU is powered up, at end of line testing. The MCU is powered up, EE_Format called, the measurements made (actually Time of Flight device calibration), and the results stored.

The headers say that's fine but in fact it can't work. So, please, which should it be, EE_Init or EE_Format? It's really not clear and it's certainly not clear that in fact EE_Format cannot be used. If the answer is EE_Init then what use is EE_Format anyway? It seems that EE_Init(EE_FORCED_ERASE) is always the preferred choice.

Sorry to labour the point but the documentation isn't clear and I'd like to contibute to it being improved to save other developers any wasted time. Many thanks


Hello @pretoriandave ,

This is an internal feedback regarding your last one:

As you correctly mentioned :
(++) Initialize EEPROM emulation, and restore the FLASH pages used by
EEPROM emulation to a known good state in case of power loss
using EE_Init(). It must be performed at system start up.

Since it must be performed at system start up, this is the first thing that needs to be called in order to setup the EEPROM Emulation mechanism.

Regarding the "it can be called the very first time EEPROM emulation is used, to prepare FLASH pages for EEPROM emulation with empty EEPROM variables."
-> that means that you can call it anytime when you're using the EEPROM emulation, but if there is no init the EEPROM Emulation can't be used (as a lot of peripherals or software mechanism).
But I can understand how you could have been misled by the header of the Format function.
Now regarding your question about the use of the Format function, you may want to flush your data or format your data without the need of a new initialization, since the init is supposed to be called at system startup and then you don't need to.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

View solution in original post

9 REPLIES 9
mƎALLEm
ST Employee

Hello @pretoriandave ,

Internal ticket 193188 for follow-up. I'll get back to you as soon as I have a feedback.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.
pretoriandave
Associate II

@mƎALLEm : A few other things for the team to consider while they are about it, if I may:

1. In the example application supplied with this middleware, there are a couple of iffy lines of code:

if ((ee_status & EE_STATUSMASK_CLEANUP) == EE_STATUSMASK_CLEANUP) {ErasingOnGoing = 0;ee_status|= EE_CleanUp();}

should surely be:

if ((ee_status & EE_STATUSMASK_CLEANUP) == EE_CLEANUP_REQUIRED) {ErasingOnGoing = 0;ee_status|= EE_CleanUp();}

It compiles the same either way, but in the spirit of improving readability, it would be better if it were changed. There are two instances of this.

2. The very next line of code is this:

if ((ee_status & EE_STATUSMASK_ERROR) == EE_STATUSMASK_ERROR) {Error_Handler();}

Not certain on this one, but think perhaps what they meant was:

if ((ee_status & EE_STATUSMASK_ERROR) != 0) {Error_Handler();}

Again, two instances.

3. Lastly, I came at this from having previously used the EEPROM emulator set out in AN3969 for older processors. This has as its example virtual addresses 0x5555, 0x6666 etc. I continued to use these for no particular reason and have spent all of today stracthing my head over why the latest stored vales are not copied across to the other page once the first is full. I now realise that the virtual addresses MUST be 1 to NM_OF_VARIABLES and therefore contiguous) for the PagesTransfer function to work. Now what's stated in AN4894, foot of page 7 about the addresses is not wrong, but it could perhaps stress this requirement more, as I managed to overlook it and others might too.

Hope these are helpful.

Hello @pretoriandave ,

This is a feedback from the package developer:

Regarding the missing CRC Config in the EE_Format function, it's not really a limitation, as described in the AN, the EE_Init is supposed to be called before any access to the Emulated EEPROM, since it's mandatory after each reset for robustness purposes in case the resets occur during a page transfer for example, so that's why the CRC Config function is not called within the format function.

But the code can be easily tailored by the customer as he seems to have done if that fit his specific use case.

Regarding the next 2 points about clarity in code we will check if an update is needed, but it doesn't imply any "bug" so that's a good news.

Regarding the last point, the virtual addresses description, it is something that has already been taken into account for next release.

Hope it does answer your question.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

@pretoriandave wrote:

I now realise that the virtual addresses MUST be 1 to NM_OF_VARIABLES and therefore contiguous) for the PagesTransfer function to work.


So that's different from the AN4061 code for STM32F0, STSW-STM32117, in which the so-called "virtual addresses" are entirely arbitrary:

https://community.st.com/t5/stm32-mcus-embedded-software/eeprom-emulation-virtual-addresses/m-p/684673/highlight/true#M48483

Presumably also for the F1, F2, F3, and F4 versions?

And WB ?

Many thanks @mƎALLEm , great service as ever. I think there may be an important distinction in here that we should bottom out, as I think it might warrant a tweak to AN4898 and/or the headers in eeprom_emul.c as they seem to be at odds...

I think what I'm gathering from the team's response is that, despite the function name, EE_Format is not how one should first format the EEPROM emulation space. In any case, without my tweak, you can't, since the CRC block is not clocked.

The response above is that calling EE_Init is mandatory after each reset and I presume that includes the very first time the MCU is powered after programming too. In other words, one should use the following to first format the EEPROM space..

EE_Init(EE_FORCED_ERASE)

By contrast, the header of eeprom_emul.c says:

(#) EEPROM emulation initialization functions:
           (++) Format the FLASH pages used by EEPROM emulation using EE_Format().
                This function is optionally used, it can be called the very first
                time EEPROM emulation is used, to prepare FLASH pages for EEPROM
                emulation with empty EEPROM variables. It can also be called at
                any time, to flush all EEPROM variables.
           (++) Initialize EEPROM emulation, and restore the FLASH pages used by
                EEPROM emulation to a known good state in case of power loss
                using EE_Init(). It must be performed at system start up.

The header suggests that EE_Format can be used to format the EEPROM space the first time the MCU is powered and the function name certainly supports that view. That is how I first did it and it didn't work for the reasons already stated. 'It can be called the very first time EEPROM emulation is used'. No it can't.

My use-case is that I am storing calibration parameters in the EEPROM emulation space which are determined the very first time the MCU is powered up, at end of line testing. The MCU is powered up, EE_Format called, the measurements made (actually Time of Flight device calibration), and the results stored.

The headers say that's fine but in fact it can't work. So, please, which should it be, EE_Init or EE_Format? It's really not clear and it's certainly not clear that in fact EE_Format cannot be used. If the answer is EE_Init then what use is EE_Format anyway? It seems that EE_Init(EE_FORCED_ERASE) is always the preferred choice.

Sorry to labour the point but the documentation isn't clear and I'd like to contibute to it being improved to save other developers any wasted time. Many thanks

pretoriandave
Associate II

@Andrew Neil Yes that's correct. AN4061 is the old method and could use arbitrary addresses. The new method requires them to be consecutive beginning at 1.


@pretoriandave wrote:

Many thanks @mƎALLEm , great service as ever. I think there may be an important distinction in here that we should bottom out, as I think it might warrant a tweak to AN4898 and/or the headers in eeprom_emul.c as they seem to be at odds...

I think what I'm gathering from the team's response is that, despite the function name, EE_Format is not how one should first format the EEPROM emulation space. In any case, without my tweak, you can't, since the CRC block is not clocked.

The response above is that calling EE_Init is mandatory after each reset and I presume that includes the very first time the MCU is powered after programming too. In other words, one should use the following to first format the EEPROM space..

EE_Init(EE_FORCED_ERASE)

By contrast, the header of eeprom_emul.c says:

(#) EEPROM emulation initialization functions:
           (++) Format the FLASH pages used by EEPROM emulation using EE_Format().
                This function is optionally used, it can be called the very first
                time EEPROM emulation is used, to prepare FLASH pages for EEPROM
                emulation with empty EEPROM variables. It can also be called at
                any time, to flush all EEPROM variables.
           (++) Initialize EEPROM emulation, and restore the FLASH pages used by
                EEPROM emulation to a known good state in case of power loss
                using EE_Init(). It must be performed at system start up.

The header suggests that EE_Format can be used to format the EEPROM space the first time the MCU is powered and the function name certainly supports that view. That is how I first did it and it didn't work for the reasons already stated. 'It can be called the very first time EEPROM emulation is used'. No it can't.

My use-case is that I am storing calibration parameters in the EEPROM emulation space which are determined the very first time the MCU is powered up, at end of line testing. The MCU is powered up, EE_Format called, the measurements made (actually Time of Flight device calibration), and the results stored.

The headers say that's fine but in fact it can't work. So, please, which should it be, EE_Init or EE_Format? It's really not clear and it's certainly not clear that in fact EE_Format cannot be used. If the answer is EE_Init then what use is EE_Format anyway? It seems that EE_Init(EE_FORCED_ERASE) is always the preferred choice.

Sorry to labour the point but the documentation isn't clear and I'd like to contibute to it being improved to save other developers any wasted time. Many thanks


Hello @pretoriandave ,

This is an internal feedback regarding your last one:

As you correctly mentioned :
(++) Initialize EEPROM emulation, and restore the FLASH pages used by
EEPROM emulation to a known good state in case of power loss
using EE_Init(). It must be performed at system start up.

Since it must be performed at system start up, this is the first thing that needs to be called in order to setup the EEPROM Emulation mechanism.

Regarding the "it can be called the very first time EEPROM emulation is used, to prepare FLASH pages for EEPROM emulation with empty EEPROM variables."
-> that means that you can call it anytime when you're using the EEPROM emulation, but if there is no init the EEPROM Emulation can't be used (as a lot of peripherals or software mechanism).
But I can understand how you could have been misled by the header of the Format function.
Now regarding your question about the use of the Format function, you may want to flush your data or format your data without the need of a new initialization, since the init is supposed to be called at system startup and then you don't need to.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.

Thanks @mƎALLEm, got it. Please can I suggest that this is clarified in the AN and the header reworded. The meaning of 'very first time' is misaleading as you have said and would benefit from being reworded. Thanks

We will take this into account for the next release. Thanks for the input.

If your questions has been answered please accept as solution the comment that answered your question(s).

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
PS:
1 - This is NOT an online support (https://ols.st.com) but a collaborative space.
2 - Please be polite in your reply. Otherwise, it will be reported as inappropriate and you will be permanently blacklisted from my help.